Instalaciones con resultados

QUICKVIC™ SD HVAC CASE STUDY:
UBC UNDERGRAD LIFE SCIENCES TEACHING LABS

University Expands Its Teaching Labs

Ubicación:
  • Vancouver, British Columbia
TIPO DE INSTALACIÓN:
  • University
PROBLEMA:
  • Modification and upgrade to current system
  • El roscado y la presión planteaban desafíos particulares
  • Maintain timeline and budget
Beneficios de QuickVic™ SD
  • Ahorro de costos
  • Facilidad y rapidez de instalación
  • Facilidad para corregir instalaciones
  • Herramientas simples
Siga leyendo

In order to maintain their reputation as a cutting-edge institution the University of British Columbia (UBC) upgraded a collection of buildings on their Vancouver campus. The renovation and expansion of the UBC Undergrad Life Sciences Teaching Labs added an extra 175,000 square feet of science labs and classrooms.

The mechanical contractor for the building, Omega Mechanical, was tasked with installing ½ - 2”/DN15 - DN50 heating and cooling lines and was planning to either thread or press Schedule 40 carbon steel pipe – joining methods the team had utilized for similar jobs in the past.

Threading and pressing presented unique challenges, including messy threading machines, expensive additional tools, and the risk of oil and metal shavings needing to be flushed out of the system. Instead, Omega opted to use the innovative Victaulic QuickVic™ SD Installation-Ready™ mechanical joining system designed for small diameter plain end carbon steel pipe, as a more efficient and economical option.

QuickVic SD products installed quickly and easily using standard tools and provided Omega with multiple visual inspection features, including bolt pad-to-bolt pad verification, a retainer inspection window, and knurled insertion depth markings on pipe ends. These features guarantee a strong, properly installed coupling or fitting. In addition, the products are engineered to allow for easy repositioning, maintenance and retrofitting without the need for joint cutouts.

“The success of the installation as it relates to both time savings and system cleanliness has been the determining factor in implementing this joining methodology to all future projects involving heating and cooling systems.”
—Brad Hedblom, President of Omega
Servicios
Hydronic Heating and Cooling
MATERIAL DE TUBERÍAS
Acero al carbón cédula 40
RANGO DE TAMAÑOS DE TUBERÍAS
½ – 2"/DN15 - DN50
Propietario
UBC Project Services
CONTRATISTA
Omega Mechanical
INGENIERO/CONSULTOR
WSP
DESCUBRA LOS BENEFICIOS DE QUICKVIC™ SD PARA SU PRÓXIMO PROYECTO
Vea más información

VEA MÁS PROYECTOS Y CLIENTES QUE SE HAN BENEFICIADO DE LAS INSTALACIONES CON QUICKVIC™ SD

REMODELACIÓN DE EDIFICIO DE DEPTOS. CON BENEFICIOS PARA LOS INQUILINOS
  • Instalación fácil y rápida
  • Mantenimiento simplificado
  • Labor Savings
Vea más información
MEJORAS EN HOTEL PARA UNA EXPERIENCIA DE MAYOR CALIDAD DE LOS HUÉSPEDES
  • Instalación fácil y rápida
  • Ahorro de tiempo
  • Mantenimiento simplificado
Vea más información
DESCUBRA LOS BENEFICIOS DE QUICKVIC™ SD PARA SU PRÓXIMO PROYECTO
Vea más información