Habla con nosotros, con tecnología LiveChat

Debunking Myths About Joining HDPE: Myth #4 – Mechanical Solutions Are Expensive

construction plans and money represent savings in mechanically joining HDPE with Victaulic instead of fusing

Debunking Myths About Joining HDPE: Myth #4 – Mechanical Solutions Are Expensive

Posted on April 11, 2018

Six Ways Mechanically Joining HDPE Will Save You Money

When it comes to joining high-density polyethylene (HDPE) pipe, mechanical solutions are a cost-effective alternative to fusion.  Mechanically joining HDPE pipe requires the purchase of couplings, but does not require any special equipment or certified workers for installation.  Reliable, verifiable joints can be created in less time, in tighter spaces, and in any orientation.  Fusing HDPE requires the capital purchase of a fusion machine, which can mean hundreds of thousands of dollars depending on the size range of the project, but that’s not the only instance in which a company will reach deep into its pockets.  With fusion comes a variety of hidden costs – things like equipment maintenance, specially trained workers, more man hours, the potential for project delays, and the need for installation space.

  1. No Special Equipment

    Mechanically joining HDPE pipe does not require the purchase of any special equipment – simple, standard tools are all that’s required.

  2. No Special Equipment Maintenance

    With the absence of special equipment comes the absence of costly maintenance of special equipment.

  3. No Certified Fusion Technicians

    Specially trained (read: more expensive) crew members are not required in order to mechanically join HDPE.

  4. Fewer Man Hours

    Up to ten times faster than fusion, mechanically joining HDPE pipe allows for confirmation of correct installation, removing the cost of joint rework.  Mechanical systems also cut out the downtime associated with heating and cooling the pipe and the time required to mobilize cumbersome equipment to move to the next joint.

  5. Less Potential for Project Delays

    With a mechanical joining solution, design changes can be made on the fly and pipe can be joined in any orientation.  Proper installation is verifiable, preventing delays due to rework.  Weather also isn’t a factor – pipe can be joined in a heatwave or in rain, snow, sleet, or hail.

  6. Less Space Required

    No need to spend money trying to get a fusion machine into a tight space or making a tight space, like a trench, bigger in order to accommodate a fusion machine.  Mechanical joints can be installed in tight spaces and narrow trenches.

Overall, comparative studies of mechanically joined and fused projects have shown the Refuse-to-Fuse™ system for HDPE to be a competitively priced option.  In a recent interview, David Sharkey, Victaulic Vice President and General Manager of Asia Pacific, said it best:  “As leaders in the mechanical joining business, we are extremely proud of the Refuse-to-Fuse solution. At Victaulic, we’re passionate about educating the market about the benefits of our mechanical joints.  Our solution exceeds HDPE pressure ratings, cuts down installation times, eliminates the need for expensive equipment and specialized workers and works in a range of underground buried and outdoor exposed conditions. What more could you want?”

We concur.  What are you waiting for?

To learn more about Victaulic HDPE Pipe Joining system performance, click here.

 


More from this series:

DEBUNKING MYTHS ABOUT JOINING HDPE: MYTH #1 – MECHANICAL JOINTS CAN’T BE BURIED OR SUBMERGED

MITOS DE LA UNIÓN DE TUBERÍAS DE HDPE: MITO #2 – LA FUSIÓN CREA UNIONES MÁS RESISTENTES

DEBUNKING MYTHS ABOUT JOINING HDPE: MYTH #3 – FUSION IS FASTER

Victaulic

Victaulic

Victaulic is the leading producer of mechanical pipe joining solutions. Engineered with confidence, our solutions put people to work faster, while increasing safety, ensuring reliability and maximizing efficiency.

Related posts

Close up view of the glass bulbs with sand running through of an egg timer or hourglass measuring passing time counting down to a deadline

DEBUNKING MYTHS ABOUT JOINING HDPE: MYTH #3 – FUSION IS FASTER

The traditional method of joining HDPE pipe is with fusion, however this process can be negatively affected by many variables. If you are looking f...

Arms holding weights - represents strength of Victaulic HDPE pipe fittings for joining HDPE pipe

MITOS DE LA UNIÓN DE TUBERÍAS DE HDPE: MITO #2 – LA FUSIÓN CREA UNIONES MÁS RESISTENTES

Victaulic's system solution for HDPE pipe is designed with strength & durability in mind. Under extreme pressure tests, Victaulic mechanical joints...

Mining Engineer in Lignite Mine

DEBUNKING MYTHS ABOUT JOINING HDPE: MYTH #1 – MECHANICAL JOINTS CAN’T BE BURIED OR SUBMERGED

Victaulic's system solution for HDPE (high density polyethylene) pipe is light-weight, corrosion-resistant, flexible, long-lasting & economical, ma...

Recent posts

HDPE Couplings Rescue a Landfill’s Failed Fusion Welds

Gas is extracted using vertical wells and a vacuum system and transported to the gas-to-energy plant via HDPE pipe before being converted into power.

Retrofit Piping Systems with Victaulic Mechanical Joining Products

The Top Six Mechanical Retrofitting Best Practices – Tip Five

Interested in the top six mechanical retrofitting best practices? Tip 5: Implement Modular Mechanical Room to Improve System Efficiency.

Large Pipe Retrofitting Job - Victaulic Best Practices - Tip Four

The Top Six Mechanical Retrofitting Best Practices – Tip Four

Interested in mechanical retrofitting best practices? Learn about the top six here here. Tip 4: Maximize Jobsite Productivity.