Habla con nosotros, con tecnología LiveChat

DEBUNKING MYTHS ABOUT JOINING HDPE: MYTH #1 – MECHANICAL JOINTS CAN’T BE BURIED OR SUBMERGED

Mining Engineer in Lignite Mine

DEBUNKING MYTHS ABOUT JOINING HDPE: MYTH #1 – MECHANICAL JOINTS CAN’T BE BURIED OR SUBMERGED

Posted on August 17, 2017

High density polyethylene (HDPE) is light-weight, corrosion-resistant, flexible, long-lasting, and economical, making it an ideal material for buried or submerged pipelines.

One of the most voiced concerns is that mechanical joints may not perform as well as fused joints in buried or submerged applications. In actual fact, Victaulic mechanical joints for HDPE pipe have been specifically designed with buried and submerged services in mind, and are perfect for many underground and underwater environments.

Constructed of durable ductile iron housings and fluoropolymer-coated, corrosion-resistant hardware, Refuse-to-Fuse™ fully restrained couplings are protected from the most challenging underground or underwater environments. If there is an area where the engineer or property owner determines additional protection is desirable, a range of industry-accepted coating and wrap options are available.

To learn more about Refuse-to-Fuse system performance, click here.

Victaulic

Victaulic

Victaulic is the leading producer of mechanical pipe joining solutions. Engineered with confidence, our solutions put people to work faster, while increasing safety, ensuring reliability and maximizing efficiency.

Related posts

Arms holding weights - represents strength of Victaulic HDPE pipe fittings for joining HDPE pipe

MITOS DE LA UNIÓN DE TUBERÍAS DE HDPE: MITO #2 – LA FUSIÓN CREA UNIONES MÁS RESISTENTES

Victaulic's system solution for HDPE pipe is designed with strength & durability in mind. Under extreme pressure tests, Victaulic mechanical joints...

Close up view of the glass bulbs with sand running through of an egg timer or hourglass measuring passing time counting down to a deadline

DEBUNKING MYTHS ABOUT JOINING HDPE: MYTH #3 – FUSION IS FASTER

The traditional method of joining HDPE pipe is with fusion, however this process can be negatively affected by many variables. If you are looking f...

construction plans and money represent savings in mechanically joining HDPE with Victaulic instead of fusing

Debunking Myths About Joining HDPE: Myth #4 – Mechanical Solutions Are Expensive

When it comes to joining high-density polyethylene (HDPE) pipe, mechanical solutions are a cost-effective alternative to fusion. Mechanically joini...

Recent posts

Victaulic Legacy Attracts the Attention of Forbes

A lot of folks will say, ‘I know Victaulic’ – but they’ve only seen one piece of what we do…” explains Luftig in an interview with Forbes.

Discover Exploring - Students from Exploring Post preparing to study engineering at Victaulic

How Did You Discover Engineering?

Victaulic engineers provide career exploration opportunities to Lehigh Valley high school students interested in engineering as a vocation.

Verbiage written on chalk board "Best Practices"

The Top Six Mechanical Retrofitting Best Practices – Tip Six

Interested in mechanical retrofitting best practices? Learn about the top six here here. Tip 6: Mechanical Noise and Vibration Control Methods.